Interface’s WTS 1200 Standard Precision LowProfile™ Wireless Load Cell is installed in the test rig. A hydraulic ram, with an installed LDVT sensor, pushes up onto the beam until it cracks or bends, and the WTS 1200 measures the forces. Data results are wirelessly transmitted to the WTS-BS-6 Wireless Telemetry Dongle Base Station when connected to the customer’s PC. The WTS-AM-2 Wireless Voltage Sensor Transmitter can also transmit results from the LDVT sensor using Log100 software.